MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STHS34PF80 – Data remains constant, TOBJECT = -48

Hello,I am trying to get the STHS34PF80 sensor working on an STM32L0 platform via I²C. My initialization sequence is as follows:Algorithm reset according to AN5867:CTRL2 (0x21) = 0x10 // FUNC_CFG_ACCESS = 1 PAGE_RW (0x11) = 0x40 // FUNC_CFG_WRITE = ...

Looking for ST MEMS & motion sensors for project

Hello, I was told by the services to check out the forum for guidance.I am working on a project that requires surface reconstruction using non-optical based solutions. I was thinking of attaching a motion sensor module to track the handheld scanner w...

ISM330DHCX and IIS2MDC connection mode 2 and pullups

 Dear sirs. I'm connecting an ISM330DHCX with an IIS2MDC and I need to know if the connections scheme is okay to operate in MODE 2Then I need to know if pullups are needed for i2c bus coming from SCx and SDx, and if pulldowns are required for INT lin...

nachus001_1-1769659288046.png

Linux I3C Slave Driver with IBI Support for LSM6DSO

Hello,My goal is to test the IBI functionality of my custom I3C master driver using the LSM6DSOX sensor. For this test, I need the Linux I3C slave driver for LSM6DSOX with IBI support. The file linux/driver/iio/imu/st_lsm6dx/st_lsm6dsx_core.c does no...

MinKi by Associate
  • 186 Views
  • 1 replies
  • 0 kudos

LSM6DSV320 FIFO configuration

Hi all,I am trying to get started with a LSM6DSV320X accelerometer, using a STEVAL-MKI251A and a Raspberry Pi 4. I can get raw Accelerometer and Gyroscope data from their dedicated output registers (0x22h to 0x2D), but when I try to use the FIFO, I c...

LSM6DSV320X Burst Read Issues

SummaryOur eventual product will use the LSM6DSV320X but right now, all we have is an LSM6DSV80X chip on the STEVAL-MK1247A breakout board. The products are close enough that I can test on the 80X. I am currently trying to implement the burst read fe...

viggydblur_0-1769783423238.png

Resolved! Anyone have v1.3.1 MEMS-STUDIO for download

Hi,We've been working on a project using v1.3.1 of MEMS Studio, but I've had to use a new laptop and it doesn't have this installed. Unfortunately, when I go to the downloads page I can only see v1.4.1 of MEMS Studio and it's forcing me to upgrade th...

SFowler by Associate II
  • 2205 Views
  • 9 replies
  • 0 kudos