MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ISM330 how is INTERNAL_FREQ_FINE set?

Hello,How is the INTERNAL_FREQ_FINE register set in the ISM330?Is it factory calibrated or is there on board logic that allows it change with age/temp/etc.?Thank you,Brandon M

BrandonM by Associate II
  • 2590 Views
  • 3 replies
  • 0 kudos

[LSM6DSOXTR] Bias drift

Hello!I took two attemps and recorded measurements in steady state (2 and 3 hours) that i want share.Config:G/XL FS: default ODR 104HzSensor data polled at rate ~ 90HzSome standby/wakeup stuff:TAP_CFG0 (56h) = b0101.0001TAP_CFG2 (57h) = b1000.0000WAK...

ruig25 by Associate
  • 3520 Views
  • 2 replies
  • 0 kudos

Resolved! "Fusion" icon not showing in Unico

Hi.I am working on evaluation with STEVAL-MKI210V2K. I use Unico to get sensor data, however what I really want is post-fusion data. Looking at other forum questions, it seems like Unico gives a "fusion" option on the left vertical tab. I don't have ...

ariy_0-1737647049593.png
ariy by Associate
  • 1276 Views
  • 1 replies
  • 0 kudos

ism330dhcx i2c get accel_x,y,z and heading calculation issue

Hi,     We are use openWRT and  ism330dhcx and LIS2MDLTR  on board.  The ko driver   has been created and  insert into kernel . When read data from  /sys/devices/platform/i2c_gpio@0/i2c-0/0-006a/iio:device2/in_accel_XXXX,   We has found the Z value i...

arprip by Associate
  • 862 Views
  • 1 replies
  • 0 kudos

LSM6DS3 FIFO data corruption on random basis.

Hi everyone! I am using LSM6DS3 in a very simple setup: For the debugging purposes I am only using accelerometer, ODR is set at 416Hz, fifo is enabled in continuous mode and set at the same freq, no decimation. Only XL data is set to be stored in fif...

oversc0re by Associate II
  • 3370 Views
  • 5 replies
  • 2 kudos

Enabling FIFO on LSM6DSOX

Hi,  I'm trying to get the FIFO working on the LSM6DSOX on a custom board with a silicon labs microcontroller, communicating both through SPI. I have checked the application note at https://www.st.com/resource/en/application_note/an5272-lsm6dsox-alwa...

amarco by Associate II
  • 9116 Views
  • 15 replies
  • 1 kudos

LSM6DSV16B voltage spikes on SPI data out

I am trying to read the data of the accelerometer and gyroscope of the LSM6DSV16B with an FPGA. I build a 4 wire SPI-Interface. I am able to write data to the chip and the chip is capable to give data out. But sometimes the output of the chip gets dr...

Screenshot 2025-01-13 092026.png
flx by Associate
  • 1107 Views
  • 2 replies
  • 0 kudos

Lsm6ds3tr_c interrupt not triggered

I use the official lsm6ds3tr-c-pid driver,Here is the code I initialized:  u8 who_amI = 0; lsm6ds3tr_c_device_id_get(&dev_ctx, &who_amI); if (who_amI != LSM6DS3TR_C_ID) { printf("lsm6ds3tr_c_device_id_get err,%d,%d", who_amI, LSM6DS3TR_C_ID); } pri...

hanjie by Associate
  • 762 Views
  • 1 replies
  • 0 kudos