2024-08-06 9:11 AM
I tried to set up a project and to do the calibration of the sensor IIS2MDC on my B-U585I-IOT02A Board I want to use MotionMC
Now the floating-point-ABI ist set to Hardware implementation and the Middleware used is the MotionMC Library MotionMC_CM33F_wc32_ot_hard.a
But when I use the function MotionMC_Initialize(sampletime, enable) it ends up in an infinite loop.
What solutions could I try to solve this?
Solved! Go to Solution.
2024-08-06 9:47 AM
Enabling the CRC Clock with one line inside MX_CRC_Init() befor the use of MotionMC_Initialize was enough:
__HAL_RCC_CRC_CLK_ENABLE();
B
2024-08-06 9:47 AM
Enabling the CRC Clock with one line inside MX_CRC_Init() befor the use of MotionMC_Initialize was enough:
__HAL_RCC_CRC_CLK_ENABLE();
B