MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi. The LIS3DHTR. I want to use the Stream-to-FIFO mode and interrupt on 'high' events to capture the 32 samples leading up to the trigger.

Am I right in saying that to make this work consistently, after each interrupt and reading out the data, you have to select Bypass mode in FIFO_CTRL_REG, and then put it back into 'Stream-to-FIFO' mode? This seems to make it work, but there's no men...

I am looking to make audio circuit

I am looking to make audio circuit. I need suggestion for microphone followed by noise cancellation ICs. Any help will be appreciated.ThanksSudhanshu.

SMeht.1 by Associate II
  • 4784 Views
  • 11 replies
  • 0 kudos

Resolved! How control Digital MEMS(MP45DT02)?

Hello, ​I am testing the MP45DT02 microphone on 32F4Discovery Board.​The final goal is to measure the sensitivity of the microphone(SPL) when you operate a buzzer with a frequency of 1 kHz.​First I set up the I2S communication as below to activate th...

0690X00000DXJx5QAH.png 0690X00000DXJlxQAH.png 0690X00000DXJm2QAH.png
DSEO by Associate II
  • 2836 Views
  • 2 replies
  • 0 kudos

Resolved! Sensor axis values are not consistent at higher ODR for LSM6DSO.

Hello,I am currently working with LSM6DSO and FIFO functionality.When ODR is set at 52Hz, axis values are correct but when I switch to 104Hz or 208Hz, values are not consistent. I have added my sensor configuration code and image to better explanatio...

0690X00000DAWITQA5.png
ASoni.2 by Associate III
  • 3594 Views
  • 4 replies
  • 0 kudos

LSM303AGR SPI Read Problem

HiI have lsm303agr mems sensor with stm32g4. It uses 3 wire SPI mode. I have problem with SPI communication. I used CubeMX with HAL mode and STMems_Standard_C_drivers for lsm303. The problem is that, when i read whoami register it reads 0x33 which is...

AAYKA.1 by Associate II
  • 2616 Views
  • 4 replies
  • 0 kudos

Not able to read accurate X, Y, Z, values of gyroscope

Hi Team,I am working with lsm6dsl 6 axis sensor , connected MT7621 processor via I2C.I would like to use gyro sensor only and followed the below setting in user space application.CTRL2_G (11h) = 0x60 (Gyro full scale 250dps, 416hz)INT1_CTRL (0Dh) = 0...

Vpava.1 by Associate
  • 1161 Views
  • 1 replies
  • 0 kudos

Why the LIS2DW12 is going into the power-down mode on restart?

(newbie)I'm configuring the registers using the STEVAL-MKI179V1 & STEVAL-MKI109V3 using Unico (see attached please)I'm planning to use int1=double_tap, int2=sleep/wakeup and to pull over spi from time to time the data (continuous mode).After i config...

0690X00000D8w86QAB.jpg
BPiti.1 by Associate
  • 1044 Views
  • 1 replies
  • 0 kudos