MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR Magnetometer result is deviated when iron comes nearby

Hi,we have used LSM303AGR  magnetometer for cupboard Door Open/Close detection and it is working properly.On door close position, i am getting ~0 of every direction as i have done hard iron compensation.Issue i am getting in small cupboard is to open...

APate.19 by Associate II
  • 3298 Views
  • 6 replies
  • 0 kudos

[LSM6DSL] Data loss during reading FIFO data?

Hi, I'm testing LSM6DSL FIFO mode. And I have a problem with output data rate.I don't have the problem with reading the data, but my problem is that average data output is about 96.5 samples per seconds while my ODR setting is 104Hz.And here is my qu...

MKang.1 by Associate II
  • 2261 Views
  • 4 replies
  • 0 kudos

SensorTile.box #NaN: Applications from all over the world

This week the winning ST.box applications of the IEEE International Contest of Sensors & Measurement Systems in Montreal, Canada, have been awarded. 1st prize application: detecting defects in steel sheets using magnetic flux generated by the ST.box ...

0690X00000DXXTxQAP.png

Avoiding (seemingly) random STMicro Motion EC Middle Ware bearing output values when the magnetometer's X axis is at a minimum.

Hi, (Was: "I would like to use STMicro Motion MC and EC Middle Ware as a normal compass while the "pitch" is positive 90 degrees.")I would like to use the STMicro Motion MC and EC Middle Ware with an LSM9DS1 sensor while the "pitch" of the LSM0DS1 is...

Rstua.1 by Senior
  • 836 Views
  • 1 replies
  • 0 kudos

Clarification on LIS3DH Event detection

Going over the application note AN3308 (Pg:27), step 9 depicts that in order to detect event, for example, free-fall, poll INT1 pad. This means checking the the physical status of the MCU pin to which INT1 pin is connected. However, looking at the ex...