2020-01-07 3:20 AM
I am looking to make audio circuit. I need suggestion for microphone followed by noise cancellation ICs.
Any help will be appreciated.
Thanks
Sudhanshu.
2020-01-08 5:47 AM
Hi @SMeht.1 , you basically need a tool (analog or digital based) to implement an active noise cancellation IC with a MEMS microphone, right? I suggest you to start from the Bluecoin kit design for the HW schematic and layout, and on the FP-AUD-SMARTMIC1 C libraries if you are starting from scratch. Regards
2020-01-09 5:26 AM
2020-01-13 6:41 AM
Hi @SMeht.1 , thanks for the invitation and the interest :) Are you specifically interest in MEMS microphone for your application on in ST MEMS sensors in general and/or for other applications (accelerometer, gyroscope, environgmental sensors?) Regards
2020-01-13 6:58 AM
Hello Eleon,
Yes I am interested only in Mems.
I was looking on ST resources. Please validate my research. I need very good quality sound and I want to remove noise from that. (If your audio processor removes noise itself, that will be good as well.)
I found following combination
1) STEVAL-MKI126V3 (ST Smart Voice)
2) STEVAL-MKI129V3 (Mems coupan)
3) STEVAL-MKI138V1 (ST audio Hub) // I feel this is required for programming audio processor STA321MP only?
Question 1: After Proof of concept, if we order STA321MP, we will get that pre-programmed or we need to program at production line?
Question 2: ST Smart Voice can give I2S output. At this I2S output, do I need another noise removing chip (may be some CODEC)? If yes, please suggest.
Question 3: My research above on ST MEMS is good for audio reception or not? i mean i need very good audio quality without noise.
If you suggest something else, please give full description.
Sudhanshu Mehta
+91-9953930827 (call me anytime)
2020-01-13 7:09 AM
Do we need anything else in for making above thing working.. I need I2S output.. Rest of things i have in place.. FYI i am looking to use WT32i bluegiga module for proof of concept.
2020-01-16 6:09 AM
Any suggestion will be appreciated..
2020-01-16 6:40 AM
I am interested in MEMS microphones
2020-01-20 2:33 AM
@Eleon BORLINI can you please help us on this?
2020-01-20 5:16 AM
@Eleon BORLINI (ST Employee)
Hello Eleon, please validate
and
are complete hardware i need for getting MEMS microphone output in I2S fotmat..