MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! steval-mki181v1 - i2c connected problem...

Hi, im have:https://www.st.com/en/evaluation-tools/steval-mki181v1.htmlI have connected after i2c in esp32. It works and sometimes disconnects it. Do you need to use any resistors?

TBart.1 by Associate II
  • 1113 Views
  • 1 replies
  • 0 kudos

Resolved! How to generate header from .ucf file?

Hello,could you please clarify one topic for me. I am working with lsm6dsox sensor. How can I create a header (.h) file instead a .ucf to easily include in a project?I read that it is possible using Unico, but i didn't find this option in it. (Unico ...

YRakh.1 by Associate II
  • 1470 Views
  • 1 replies
  • 0 kudos

Resolved! Programming the sensor tile

Good day,I have purchased a sensor-tile and would like to code said tile. The board is receiving power and the SWD connections are correct and double checked. Then when the st link is plugged in and one wants to debug and program the micro an error s...

FBoth.1 by Associate III
  • 5002 Views
  • 8 replies
  • 0 kudos

lsm6ds3 Relative tilt function

the first interrupt is generated if the device is rotated by an angle greater than 35 degreesfrom the start position and remains in the blue zone for a period of time of at least 2 seconds1�?35 degrees. What is its principle calculation formula?At le...

ZhangTao by Associate II
  • 4651 Views
  • 7 replies
  • 0 kudos

LIS2DH12 zero-g level offset.

Hello everyone,I'm using lis2dh12 for acceleration measurement. In the datasheet, I find the typical zero-g offset accuracy is +/-40mg. When the device is placed horizontally, the reading of X-axis and Y-axis should be 0. For most of our devices, the...

lbing.1 by Associate II
  • 1522 Views
  • 2 replies
  • 0 kudos