MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH accelorometer based on i2c

Hi,we are woeking on motion detection application using LIS3DH,we have done below registersettings but we are only getting interrupt on motion first time but after that we are not getting interrupt after reset also.once we are getting th einterrupt a...

AKUMA.1 by Associate
  • 1302 Views
  • 2 replies
  • 0 kudos

ERROR MESSAGE

HI everyone, I have this error message when I compile my main program with eclipse ... I'm using a P Nucleo 53L0A1 .. someone can tell me what's happening because I really don't understanderror message =>Open On-Chip Debugger 0.10.0+dev-00021-g524e8c...

MSAMB.1 by Associate III
  • 949 Views
  • 1 replies
  • 0 kudos

LPS22HB address?

Hi.I'm testing pressure using LPS22HB IC.I connect GND SD0.But LPS22HB give me address nack.So I change address "Low" to "High", LPS22HB give me strange pressure value and not address nack.Why do LPS22HB address strange?Thank you.

JLee.21 by Associate II
  • 3308 Views
  • 6 replies
  • 0 kudos

What is modulus of acceleration?

In Design Tip DT0106, is it mentioned that:Another technique which can be of help in controlling the integration error is known as Zero-Velocity-Update (ZVU): when the modulus of the acceleration is 1g and the output of the gyroscope is near 0, then ...

NLe.1 by Associate
  • 2024 Views
  • 2 replies
  • 0 kudos

Transferring PDM_OUT from MP45DT02 to CS43L22

I want to access PDM_OUT data from the MP45DT02 and output this on the CS43L22. For this I want to use the I2S protocol but I have difficulties connecting the MP45DT02 to the I2S mode and using the HAL_I2S_Receive function. How do you initialize the ...

JtotheF by Associate
  • 1055 Views
  • 1 replies
  • 0 kudos

VL53L0X CALIBRATION

Hello, I am writing this message to you because I need help, if it is possible I would be grateful to you .. Ok, I am working on a project in which we will use the VL53L0X as a sensor in an access control device , we will use it as a proximity sensor...

MSAMB.1 by Associate III
  • 850 Views
  • 0 replies
  • 0 kudos