User Activity

I have been working with this sensor for a while. It started to give weird errors such as reading all zeros on all axis. Then sometimes it would initialize but read values like 4, 0, 4 and such. Which is impossible in a static position. I have tried ...
Hello, I would like to know if there are any special tricks to SPI half-duplex mode. As far as I know the configuration is done normally with only the direction as 1 line. Can anyone point me to some form of an example for setting up the SPI in half-...
Good day,I have purchased a sensor-tile and would like to code said tile. The board is receiving power and the SWD connections are correct and double checked. Then when the st link is plugged in and one wants to debug and program the micro an error s...
Kudos from