MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sending large amount of data with USB

I'm currently facing a big problem. I've an MCU (STM32L4) connected to an SD card (SDIO) which stores tons of data (5Gb) from a microphone (ST MEMS). I need to send this data as fast as possible from SD card to my PC. With a serial port this is to sl...

MAndr.233 by Associate III
  • 8883 Views
  • 11 replies
  • 0 kudos

Resolved! LSM6DS3 pin capacitance

Hi,I am using the LSM6DS3 with I2C at 400 kHZ. I would like to know the pin capacitance value so as to calculate the value of the required pull up resistors. I was unable to find this in the data sheet.Thanks

GTS.1 by Associate III
  • 1827 Views
  • 3 replies
  • 0 kudos

Resolved! LSM303AGR date code?

Hi,I would just like to know the date code on the LSM303AGR on our PCB Board. So far I have not found any document to interpret the date code. The markings are 636 AGR.Regards,Markel

0693W000003C0CrQAK.jpg
MRobr by Associate III
  • 2448 Views
  • 4 replies
  • 0 kudos

LIS2DE12 pull up resistor values

Hi,I have been using the LIS3DH successfully but I want to go to the LIS2DE12 because it is smaller and only does what I need. I have wired up a STEVAL-MKI175V1 board to a 3.3 v Arduino close to do some initial evaluation. I can't get it to respond a...

RKeit.1 by Associate III
  • 2298 Views
  • 4 replies
  • 0 kudos

Dont getting data from max30100 connected to NUCLEO F401RE

Hello,I connected the nucleo F401RE to max30100 using i2c level shifter tca 9406 https://www.ti.com/lit/ds/symlink/tca9406.pdf?ts=1596413075744, and I am only getting the adderss of the sensor but no data.I also tried to add 10k resistors and got t...

YBuch.1 by Associate III
  • 1483 Views
  • 1 replies
  • 0 kudos

VL53LDK Index address ?

Hello?I have a question.I am developing using MCU.I am using VL53LDK to measure distance.I want to know the I2C Index address.Index address:?How many byte?How can i calculation?Thank you.

DJang.1 by Associate
  • 2694 Views
  • 1 replies
  • 0 kudos

Use LIS2DH12 detect sit or stand

Hello everyoneWe are designing a wearable device. It's worn on the waist. We want it can generate an interrupt when a man sit down or stand up, so that we can know a man is sitting or standing. It's a low-power device, wake up every 3 seconds.Now, we...

lbing.1 by Associate II
  • 1546 Views
  • 2 replies
  • 0 kudos

LIS2DH12 fault

Hello everyoneOur device use lis2dh12 to measure the acceleration. We tested 10 boards. But we find 3 board work abnormal. These three board are all facing up, the reading of x axis and y axis should be 0, and z axis should be 1g. But the readings o...

lbing.1 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

Resolved! which spi mode is supported in iis3dwb sensor and why it fail to read who am i register at first attempt after reset?

I am exploring iis3dwb sensor with stm32f401 nucleo board.i go through the data sheet but not find any information which mode this sensor supported?so i tried with these 2 setting , hspi3.Init.CLKPolarity = SPI_POLARITY_LOW; hspi3.Init.CLKPhase = SPI...

karan by Associate III
  • 3730 Views
  • 1 replies
  • 0 kudos

LPS22HB non-volatile calibration ?

I'm currently using the LPS22HB pressure sensor in order to make a CO2 sensor more accurate. We need to calibrate the pressure sensor so it doesn't incorrectly modify the CO2 reading. We are having difficulty understanding wether the one point calibr...

JDart.1 by Associate
  • 1259 Views
  • 1 replies
  • 0 kudos