MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2MDL false pulse generation

Greetings! I am using the LIS2MDL magnetometer in continuous mode (10 Hz) with hard-iron offset and interrupts enabled. (Full settings: CFG_A: 0x90; B: 0x0A; C: 0x50; INT_C: 0xE5) And I am trying to detect a magnetic object coming near the device. Th...

MarkMan_0-1775824923000.png
MarkMan by Associate II
  • 199 Views
  • 3 replies
  • 0 kudos

Resolved! FSM "dual" timer for fail-safe

Hi.I'm working with the FSM in LSM6DSO. I'm able to program detection which I want, but I struggle to do something like "fail-safe" to avoid the algorithm to stuck in the middle of the detection.For example, I want to do a "throw" detection of a thin...

image.png
Bennny by Associate III
  • 244 Views
  • 2 replies
  • 0 kudos

STEVAL-PROTEUS1 to monitor temp and vibration on a spindle

Hello,  I am trying to use a proteus1 to monitor temp and vibration on a spindle and i just cant seem to find the best way to do this. I would  like to use a cloud so I can monitor it off site and get a notification if the temp rises above a threshol...

Cornwlp by Associate
  • 226 Views
  • 2 replies
  • 2 kudos

MotionFX output stuck at zero on STM32L476 Discovery

Hi everyone,I am struggling to get MotionFX (9-axis sensor fusion) working on an STM32L476G-DISCOVERY board using the onboard LSM303C (Acc/Mag) and L3GD20 (Gyro).The Problem: Despite the library being initialized and updated in the main loop, all out...

Resolved! Lis3dh : X Y & Z value and Threshold configuration

Hello,I have two technical questions regarding the lis3dh accelerometer behavior and interrupt configuration.1) Are the values I read from the LIS3dh  in m/s²????  Exemple :::Accel [LIS3dh] 28807220458ns (-7.300384, -1.942303, -5.712095)2) Interrupt ...

ASREB by Associate
  • 136 Views
  • 1 replies
  • 1 kudos

Accelerometer zero-g level change over time

Hi,I am using IIS2ICLX MEMS accelerometer in an IOT device.The IIS2ICLX is soldered on a PCB that sends data to internet every 10min.To measure the zero-g level of both x and y axis, I suspend the device from the ceiling so that the PCB (and the acce...

Resolved! ISM330DHCX Measurement

Hi. I have been looking at the internal operation of MEMS devices and am looking for information on how this sensor takes the reading from the mechanical parts. I am trying to find out if this sensor uses capacitive sensing or frequency drift and tim...

jhurd by Associate
  • 84 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSV320X sensor not responding

Hello everyone. I would really appreciate if someone could help me sort out a really annoying issue i have with a new STM32WB5MMGH6 based board i made.On this board i have two sensors connected to the same SPI interface (hspi2) with different CS pins...

Screenshot 2026-04-15 at 14.24.40.png Screenshot 2026-04-15 at 14.25.41.png Screenshot 2026-04-15 at 14.29.50.png Screenshot 2026-04-15 at 14.31.57.png
yaxsomo by Associate III
  • 232 Views
  • 3 replies
  • 2 kudos