2025-12-22 12:48 AM
In the datasheet of LSM6DSV80XTR maximum junction temperature is not mention. Maximum junction temperature is required to do the thermal calculation. please any guidance how to obtain the maximum junction temperature till which this IC can work safely.
2025-12-22 1:16 AM - edited 2025-12-22 2:15 AM
>the maximum junction temperature till which this IC can work safely.
See ds :
As its a low power device , Operating temperature range is the limiting factor .
More "thermal calculation" makes no sense.
+
>what is the junction temperature of the LSM6DSV80XTR
= ambient temp.
2025-12-22 2:29 AM
See also: LSM6DS3TR-C thermal charactersitics.