2025-11-04 4:10 PM
Datasheet 4.5 Maximum value for Symbol Vin in Absolute maximum ratings is 0.3 to Vdd_IO +0.3, should it be -0.3 to Vdd_IO +0.3?
Solved! Go to Solution.
2025-11-06 2:39 AM
Ciao @ggob ,
It means that you have to multiply VDDIO by 0.3.
2025-11-06 2:39 AM
Ciao @ggob ,
It means that you have to multiply VDDIO by 0.3.
2025-11-06 3:58 PM
If the VDDIO voltage is 3.3V, it means that adding a signal less than 0.99V may break it.
Is this true?
2025-12-22 6:50 AM
Yes, correct.