MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to program STEVAL-BCN002V1B?

Hello! Thank you in advance for your help =)I've just bought a STEVAL-BCN002V1B (BlueNRG - Tile), with the host board to Flash and debug, and i would like to know how i can easily program it. Questions:I've found this video where a STEVAL-IDB007V1 ...

0693W000005BQFiQAO.jpg 0693W000005BQHAQA4.png
DDi L.1 by Associate
  • 2747 Views
  • 2 replies
  • 0 kudos

STM ToF sensor (VL53L1) vs VL53L1X

Hi ST Micro, I have tested the X-CUBE-53L1A2 software with X-NUCLEO-53L1A2 expansion board, I cannot get ranging measurement above 4m using Lite Ranging or Autonomous mode (16x16 ROI). Then I tested the X-CUBE-53L1A2 software with X-NUCLEO-53L1A1 exp...

Ct.1 by Associate
  • 1575 Views
  • 0 replies
  • 1 kudos

Resolved! FTP Client Example for STWIN STEVAL

Hi Everyone, Is there any example for FTP Client on STWIN eval board? If yes, please share. Thanks much in advance@Eleon BORLINI​ any suggestion from you?Is there any Third Party library which I can use?Kind RegardsChandra

Resolved! AlgoBuilder: Create a new firmware template

Hi,my goal is to use custom template files in AlgoBuilder. For instance have an extra function or class in the main.c file. Therefore I would like to create a new firmware template for NUCLEO-L476RG as described in en.UM2689.I am working with CubeMX,...

AKato.1 by Associate II
  • 5819 Views
  • 8 replies
  • 0 kudos

Resolved! Info about sensortile capabilities

Hi,I need to get accelerometer data with a frequency of 100hz and I'm looking for the sensortiles STEVAL-STLKT01V1Looking at the documentantion is not clear to me what is the data sample rate they have by default.Here in the community someone mentio...

ADe C.1 by Associate II
  • 2502 Views
  • 5 replies
  • 0 kudos

Resolved! Max. OUT Value for LIS2DS12 not as high as expected

We are using the LIS2DS12 in an environment where we sometimes exceed the configured range (i.e +- 8g).We would expect to be the positive maximum OUT Value to be 0x7FFC and the negative maximum to be 0x8000. Instead the + max value is 0x7FE0 and neg...

glalex by Associate
  • 1019 Views
  • 1 replies
  • 0 kudos

Resolved! Information regarding LIS2DS12 accelerometer

Hi,I am a post-doctoral researcher at the University of Northampton doing research on a special type of structure. As a part of our current project, I need to measure the vibration of the structural components, and I would like to use LIS2DS12 accele...

MMojt.1 by Associate
  • 1028 Views
  • 1 replies
  • 0 kudos

How do I interface with STEVAL-MKI128V6 sensor module on Android?

Hello,I have purchased Lantronix Open-Q™ 2500 Development Kit:https://www.lantronix.com/products/open-q-2500-development-kit/#tab-featureswhich features a Qualcomm Snapdragon™ Wear 2500 (APQ8009W) optimized for wearables and a Quad-Core ARM Cortex A7...

OCohe.2 by Associate
  • 1441 Views
  • 1 replies
  • 0 kudos