MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi , I like to use NUCLEO-L476RG's DAC output to output audio from analog and digital microphones. Can I stack both AMICAM1 and CCA02M2 modules on Nucleo-L476RG at the same time?

Which board should supply the power to the system?I am using AMICAM1 to power the NUCLEO-L476RG following the instruction. AVDD is provided by AMICAM1 because the SB57 on NUCLEO-L476RG has been removed. Will a powered AMICAM1 module also supply power...

WDai by Associate II
  • 3314 Views
  • 7 replies
  • 0 kudos

Resolved! Need advice to redesign and reprogram a STEVAL-STWINKT1 board

I wish to make changes to a STEVAL-STWINKT1 which I bought, in other words I have to redesign to suit my application. The example projects works fine. I want to know from experts, is there a tool which will help me to write program or copy the exampl...

Shaun.t by Associate III
  • 3480 Views
  • 9 replies
  • 0 kudos

motion fx library running at 100hz giving wrong orientations when the device attached to it rotates at faster speeds

I'm using motion fx library to get orientation of the device. I'm putting the device running sensor-fusion on a cricket bat. If I play a very fast swing, the orientations are becoming inaccurate. if I wait for some time holding bat in standstill p...

Resolved! Erratic results from magnetometer

I have an application using a LSM9DS1 with the purpose of accurately measuring the rotational speed of a platter spinning at about 33 rpm.I measure the speed by taking readings from the gyroscope every 10ms. I did an initial calibration for offset an...

PRebo.1 by Associate II
  • 1385 Views
  • 1 replies
  • 0 kudos

Flexible Tilt angle measurement/interrupt in LIS2DW12

Hi ,. I uses LIS2DW12. I have seen that 6D orientation angle is from 45 or 50 degrees only. So setting an interrupt for this wont be useful for my purpose.I would like to wake up on minimum angle that I sets, say 5degree/10 degree . How could I achie...

Vsv.1 by Associate II
  • 7103 Views
  • 14 replies
  • 0 kudos