User Activity

Hello ST Community,I am using LIS2DH12 sensor for the following purpose: Generate an interrupt when the acceleration exceeds 1.7 g in any axes and read the x, y and z-axis values after the interrupt is generated. Generate an interrupt when the accele...
Hello ST Community,I have some hardware samples with LIS2DH12 accelerometer. For all the samples except one, the value of WHO_AM_I register is read as 0x33 (which is expected). However, for one of the samples, it is read as 0xFF. What could be the po...
Hello ST community,I would like to know how to detect the following motion using 6D function in LIS2DH12. From the application note, I understand the kind of movements detected. However, the motion that I would like to be detected is as shown in the ...
Hello ST community,I am exploring the use of LIS2DH12 for an application where I need to detect positive peak of 200 mg and negative peak of -150 mg. For this, I am planning to use the two interrupts INT1 and INT2 for positive and negative peak dete...
Hello ST community,In LIS2DS12 application note, section 5.9.1, it is mentioned that the minimum threshold can be set where 1 LSB = FS/64. I would like to confirm if the value in this register has the unit of g. Also, if +- 2g is the selected full sc...