MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it an error in the datasheet of lsm6ds3tr-c?

As the datasheet wrote, the full scale of angular rate measurement range is 2000 dps, and the output value is a 16-bit word in two’s complement, so when we set the angular rate measurement range to 2000 dps, the sensitivity (unit mdps/LSB)could be ca...

0693W00000GZA2VQAX.jpg
BChao by Associate II
  • 1753 Views
  • 2 replies
  • 0 kudos

LIS2DTW12 Threshold setting

Hello,I read the application note related to the LIS2DW12 (AN5038) and the point 6.5 confused me : On the table is recommended to set FTH_THS at 8 if the ODR is 200 Hz and I2C is running at 100KHz.A sample of 3 acceleration (6 bytes) is read in 830 ...

0693W00000GYoAmQAL.png
RStra by Associate III
  • 868 Views
  • 1 replies
  • 0 kudos

HTS221 Incorrect Temperatures / Calibration (T0_OUT = 0)

Hi,I'm having an problem whereby I believe the temperature readings from an HTS221 device are incorrect. They seems to be around 5degC too high compared to reference temp. I'm using a Nest thermostat as the reference, and while this may not be calibr...

Simon Sq by Associate III
  • 6065 Views
  • 12 replies
  • 0 kudos

Resolved! I got the MLC working on the lsm6dsox. But when i enable stepcount on FIFO my MLC stops working ? these are the 3 lines , is there anyway i can use MLC and stepcount? or will i have to make my own step count tree?

/* Start Machine Learning Core configuration */    for (uint32_t i = 0; i                               sizeof(ucf_line_t));         i++)    {        lsm6dsox_write_reg(p_lsm6dsox, lsm6dsox_MLC[i].address,                           (uint8_t *)&lsm6ds...

MJurk.1 by Associate
  • 1828 Views
  • 3 replies
  • 0 kudos

Resolved! Hi. I'm trying to make a very slight modification to the SensorTile_ALLMEMS1 project. I want to be able to read the ACC_GYRO_MAG char value over BLE.

In the sensor_service.c source file, I add the char_prop_read flag in the below, but now the SensorTile does not even start BLE properly. Any help is appreciated.starting at line 1074, COPY_ACC_GYRO_MAG_W2ST_CHAR_UUID(uuid); ret = aci_gatt_add_char(...

MCoop.1 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSL data not correct

Lsm6dsl reads out the data, and the z-axis data is always biased. When the acceleration range is set to 2G, it is placed vertically on the ground, and the z-axis is upward. The data is:Acceleration [mg]:30.68 106.32 1998.60the z-axis is down​Accelera...

oning.1 by Associate
  • 1614 Views
  • 2 replies
  • 0 kudos