MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSL data not correct

Lsm6dsl reads out the data, and the z-axis data is always biased. When the acceleration range is set to 2G, it is placed vertically on the ground, and the z-axis is upward. The data is:Acceleration [mg]:30.68 106.32 1998.60the z-axis is down​Accelera...

oning.1 by Associate
  • 1673 Views
  • 2 replies
  • 0 kudos

MotionDI precision issue when translating the sensor

I'm using the MotionDI "dynamic inclinometer" library with a LSM6DSOX (on a NUCLEO-L476RG). The rotation computed by the library looks right as long as the sensor remains stationary. But when I translate the sensor, there is a temporary but significa...

paul19 by Associate III
  • 2611 Views
  • 4 replies
  • 0 kudos

ADC + DMA for Analog Microphone. I am using Sensortile.BOx STEVAL - MKSBOX1V1 Kit. 1. Is sampling rate for Calculation is correct 2. I have configured DMA + ADC - Kindly confirm whether configuration is ok. 3. How to read DMA Data and send to UART

ADC Sampling rate :-Total Conversion Time (Tconv) = Samplingtime + 12 (This 12 is for 12-bit resolution of ADC). If I set 12.5 Cycles in MX based on the settings of the controller STM32L9RI My ADCCLK Cycle will be =24.5 . Please confirm whether 12 to...

0693W00000GYby1QAD.png 0693W00000GYc7HQAT.png 0693W00000GYc7qQAD.png 0693W00000GYc8UQAT.png

SensorTile Box - Setup

Hello,We have purchased the Sensortile box as we were told it was able to measure G-Force deceleration from an impact and display this in the number of "G's" the crash was.We understand it has a built in accelerometer and gyro's but I am unsure of ho...

ZBarn.1 by Associate
  • 1341 Views
  • 2 replies
  • 0 kudos

Resolved! IIS3DWB minimum bandwidth

Hi,I am a little confused at the datasheet for the IIS3DWB bandwidth. I clearly can see that the maximum frequency is 6.3kHz. However, is there a minimum measurable frequency? On the pg.1 features summary is says "Ultra-wide and flat frequency respon...

JChar.2 by Associate
  • 2268 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DTW12 wake up filter

Hello,I want to monitor signals in range 0.5 - 80 Hz to wake up a microcontroller on INT1 pin when acceleration is above a certain threshold.My setup is :ODR = 200HzFS = 2GMODE = Low power mode 4, Low NoiseBW_FILT = 00 --> ODR/2 --> 100HzWK_THS = 1 ...

RStra by Associate III
  • 2191 Views
  • 3 replies
  • 0 kudos

Resolved! FIR filter for MEMS

Hello,Are there any examples for implementation FIR filter on accelerometer and gyro data with programmable cut-off frequency? It would be better if CMSIS DSP functions are used.

JDave.4 by Associate III
  • 2511 Views
  • 3 replies
  • 0 kudos