2021-08-01 1:28 PM
Hi all,
I'am working with a LSM6DSO32, and I try to implement AHRS algorithm to fuse gyro and accel data. In source code I have this line
FusionVector3 gyroscopeSensitivity = {
1.0f,
1.0f,
1.0f,
}; // replace these values with actual sensitivity in degrees per second per lsb as specified in gyroscope datasheetSo if I've understood well, for my LSM6DSO32 configure at 500dps, I have a sensitivity at 17.50 mdps/LSB, so mdps is milli degrees per second that's right ? So in my struct I have to replace 1.0f by 0.0175f am I right?
Thanks
Solved! Go to Solution.
2021-08-02 7:49 AM
Hi, right, it should be the 3 axis sensitivity. If you are working at FS=500dps, the calculation is the one you have reported.
Tom
2021-08-02 7:49 AM
Hi, right, it should be the 3 axis sensitivity. If you are working at FS=500dps, the calculation is the one you have reported.
Tom