MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lsm6dsl too high power consumption problem

Operating Voltage:3.3VThe initial configuration of lsm6dsl is as follows/** * @brief Initialize the LSM6DSL sensor * @param pObj the device pObj * @retval 0 in case of success, an error code otherwise */ int32_t LSM6DSL_Init(void) { /* Enable...

Slong.1 by Associate II
  • 1315 Views
  • 1 replies
  • 0 kudos

Resolved! lps27hhw problem with negative temperature

HelloWe use the lps27hhw in our devices. When temperature is positive - all right. But when temperature is negative - the sensor sends the temperature less than it actually is (example -40* instead -20*). I put the appliance in the freezer, the tempe...

0693W00000HntqmQAB.jpg 0693W00000HntrpQAB.jpg 0693W00000HntrkQAB.jpg
DPesk.1 by Associate II
  • 2813 Views
  • 4 replies
  • 0 kudos

LIS2DW12TR Accelerometer X, Y, Z values always return 0

Hi ,guys:I have use the following code to read accelerometer data but the sensor data X, Y, Z are always 0 and I check register WHO_AM_I and it is quite correct. And I also check Status register but the DRDY always 0(means Sensor data not ready).uint...

NWang.1 by Associate II
  • 1512 Views
  • 2 replies
  • 0 kudos