MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DWB ESP32

Hello all,I would like to try to use the IIS3DWB with ESP32 with SPI. I found very few resources over internet and I tried to use the generic driver from ST github but with no luck. Anyone has a working example I can use?Thank you!

LBurc.1 by Associate
  • 1754 Views
  • 2 replies
  • 0 kudos

Resolved! Is the LIS302DLTR Accelerometer still available to buy somewhere or is there a replacement product with the same package ?

Good morning,For the company I'm working for (the CEA in Grenoble), I need to rebuild an electronic device of an old project.In order to build the PCBs, I'm looking for a specific accelerometer: the 3-axis accelerometer "LIS302DLTR" with a LGA packag...

AMOND.1 by Associate II
  • 4788 Views
  • 7 replies
  • 0 kudos

Resolved! What is MEMS sensor hardware self test principle?

 Dear all:From this diagram we can see that, gyro test is calculate whether the difference between the two data values is within the range.I want to know Write 04h to CTRL5_C (14h) Enable, What does the hardware do? What does it mean if the data ...

0693W00000HnkapQAB.png
YSONG.1 by ST Employee
  • 2276 Views
  • 2 replies
  • 0 kudos

UNICO GUI VISUALIZATION PROBLEMS

Hi All,I have installed UNICO GUI 9.9.0.0 to evaluate evibrations.I have some problems in plotting values< it seems that the graphic interface does not work correctly.I attach an image to show you the problem.OS: W7 PRO on Intel i3-2120 -- Integrate...

0693W00000AOH8tQAH.jpg
FCern by Associate II
  • 1922 Views
  • 5 replies
  • 0 kudos
LBord.1 by Associate
  • 1614 Views
  • 2 replies
  • 0 kudos

Resolved! IIS2DH aliasing at low ODR settings

AFAIK the IIS2DH has no anlog anti aliasing filter. So will aliasing occure if I use low ODR settings and the input signal is frequency is higher than ODR/2? Because in our test we are getting quiten often spikes in the signal output signal. And if t...

THart.14 by Associate II
  • 2165 Views
  • 4 replies
  • 0 kudos