I am using LSM6DSL , configure 2g 416 odr.I read the accelerometer once every 1 sec without using CTRL1_XL register.I get y axis changes from -378 to -152 , Result about 2 degrees change..Is the output of acc x,y,z valid between ODR reads ?
Hi.What if I must have Double Tap and Step Counter at the same time .Can I use " 28h to CTRL1_XL " for Double Tap and Step Counter ?.I will use 6D orientation when Double Tap and Step Counter are not necessary .Please Advise