I want to know if i open acc or gyro odr twice in diffrent time,how will mems work. (twice odr is the same)Question: Whether the MEMS will reset? Or if the last state is the same as now, nothing will be done?
Dear all:From this diagram we can see that, gyro test is calculate whether the difference between the two data values is within the range.I want to know Write 04h to CTRL5_C (14h) Enable, What does the hardware do? What does it mean if the data ...
Our custmer want to free design gesture or other motion detect. who can share some documents about filter configuration and features setting. When to use what filter, and when to use what features?
Yes, i also have the same problem. I'm also looking for answers. Use printf will print nothing.#include "main.h"#include "stdio.h"/* Private includes ----------------------------------------------------------*//* USER CODE BEGIN Includes *//* USER CO...