MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

cannot get the lis3dh to generate interrupts for new data ready

We switched from a Bosch BMA456 to the LIS3DH, and cannot get the device to generate an interrupt, we have followed the DS and app note, nothing. This solution worked with the previous device.We need assistance, this should work, the name reads corr...

Herb by Associate
  • 1327 Views
  • 1 replies
  • 0 kudos

H3LIS331HDL Z Axis reading high in static environment

Hello All,We're having some trouble with our H3LIS331HDL and I'm hoping someone can point us in the right direction.Below is a recording from a device with the high-G issue on the Z-axis. The device is in a static position on a desk and we're seeing ...

0693W00000HpafKQAR.png 0693W00000HpafPQAR.png
BTatt.1 by Associate
  • 1406 Views
  • 2 replies
  • 0 kudos

Resolved! X-Nucleo-IKS01A2 and Nucleo-L496ZG

Hello,I would like to know about the integration between Nucleo-L496GZ with X-Nucleo-IKS01A2 sensor board.Is there really no example that facilitates the integration of these boards?There really is no example using the Nucleo-L496ZG integrated with s...

GThab.1 by Associate II
  • 1400 Views
  • 1 replies
  • 0 kudos

Is VL6180X really a stable sensor in practice?

Hi,I am using VL6180X sensor in project to detect hands or other objects, without using API. I am setting registers myself. One thing that is really disappointed me regardless of other amazing features, is the interrupt and flags. Whenever the interr...

ashah.16 by Associate II
  • 1552 Views
  • 1 replies
  • 0 kudos

Reading from LIS3MDL interrupt fails the second time.

Hey All,I'm trying to read from an LIS3MDL after a threshold interrupt. While I configure everything ok and receive interrupts the chip only responds to the first event. All subsequent events fail. Here's the setup:write to 0x1C ack data: 0x0F read t...

0693W00000GXyjGQAT.png 0693W00000GXyjLQAT.png

Resolved! LIS2DH12 current consumption in the Low power .

Hello folks,I am trying to interface LIS2DH12 with NRF52840 DK(nordic semiconductor's Development Board )by using SPI bus protocol for which I have used the ST drivers from the link below,https://github.com/STMicroelectronics/STMems_Standard_C_driver...

ASing.15 by Associate II
  • 1728 Views
  • 2 replies
  • 0 kudos