MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! asm330lhhx scale factor for each x, y, z axis

Hello,For the asm330lhhx device, when does the scale value change and get set?  I am trying to determine if the scale factor needs to be checked only once at power up or continually while reading the raw x, y, and z values for both the gyro and the a...

Resolved! LSM6DSV Sensor Hub current consumption?

Based on power measurements I infer that using the LSM6DSV embedded SensorHub with a single slave (LPS22DF) costs ~6.4 uA. I can't find the expected current consumption for the LSM6DSV Sensor Hub in the data sheet or application notes. Is this a reas...

KWine by Senior
  • 2430 Views
  • 3 replies
  • 0 kudos

Resolved! Documentation for MEMS module

Where can I find the proper documentation for the functions in X -Cube - MEMS package and clear explanations for the use of functions

Priyaa by Associate II
  • 1375 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DUX12 not reaching current consumption said in datasheet

Hello,I'm evaluating the LIS2DUX12 accelerometer by using the combination of STEVAL-MKI109V3 and STEVAL-MKI238A. In the datasheet it stablishes that it can reach down to 10 nA during deep power-down:But when I measure the current consumption through ...

sch0bert_0-1695906333273.png sch0bert_1-1695906513982.png
sch0bert by Associate III
  • 3939 Views
  • 6 replies
  • 0 kudos

Resolved! Can't get to find how to turn off temp sensor from LIS2DUX12

Hello! I'm evaluating the LIS2DUX12 accelerometer by using the combination of STEVAL-MKI109V3 and STEVAL-MKI238A. In the datasheet it stablishes that in order to achieve certain current consumption is necessary to have the Temperature sensor off:But ...

sch0bert_0-1695906928646.png
sch0bert by Associate III
  • 3924 Views
  • 7 replies
  • 1 kudos

Resolved! LIS3DSH, SDO Pullup Register

Hello,We have been using the LIS3DH for some time and recently acquire some LIS3DSH' as well.With both modules there is an internal pull-up for the SDO pin, and with the LIS3DH there is a register to control this pullup:CTRL_REG0I am not able to find...

videojames_0-1695096274516.png

Resolved! FSM compatibility with SFLP or tap detect in LSM6DSV?

I have four FSM programs working with the LSM6DSV sensor, all set to AODR/GODR of 30Hz in line with the examples I copied. Tap detect requires significantly higher ODR.  I might also want to run the SFLP at a rate higher than 15 or 30 Hz, so does thi...

KWine by Senior
  • 2266 Views
  • 3 replies
  • 0 kudos

LIS3MDL hard iron offset registers

 Hi, the datasheet for the LIS3ML does not mention any dedicated offset registers that can be used to deduct an offset vector from the measurements: However, when I view the LIS3MDL app note, it says they are there: The app note points to 05h through...

Schermafbeelding 2023-10-16 om 14.59.54.png Schermafbeelding 2023-10-16 om 15.01.33.png

Resolved! LSM6DSV16X chip does not work.

LSM6DSV16X chip does not work.I purchased the LSM6DSV16XTR chip, then looked at the datasheet and built a simple circuit.But SPI communication doesn't work.I used the LSM6DSV16X arduino library provided by Sparkfun, but communication was not possible...

스크린샷 2023-10-14 151432.png 스크린샷 2023-10-19 202215.png
YJU by Associate
  • 3096 Views
  • 3 replies
  • 0 kudos