User Activity

Hello,I noticed that INT2 is repeated in 2 pins so it confuses to identify which is INT1 and INT2. Please consider change it for future production. Regards,Pascal.
Hello,I'm interfacing the STEVAL$MKI238AA through serial commands with STEVAL-MKI109V3. The UM2116 document in its Rev 10 - April 2022 doesn't mention any reference to the LIS2DUX12. I would like to know what is the format when I send the command *st...
Hello,After generating my ucf file that I load to my LIS2DUX12 and verify that it works, I wanted to load the generated configuration through a microcontroller so I used the option in Unico GUI to generate the header file which later on I need to inc...
Hello,I'm considering to use NanoEdgeAI generated model in a Zephyr project but I haven't been able to find any integration with it. I have been trying to integrate it using cmake but I'm having issues to do it (not the same math library, not finding...
Hello, I generated a nClassification model using the LIS2DE12 accelerometer through NanoEdgeAI Studio but when I try to integrate it to my project using VSCode I get the next error:c:/ncs/toolchains/31f4403e35/opt/zephyr-sdk/arm-zephyr-eabi/bin/../li...
Kudos given to