Skip to main content
KWine
Senior
October 1, 2023
Solved

FSM compatibility with SFLP or tap detect in LSM6DSV?

  • October 1, 2023
  • 3 replies
  • 1387 views

I have four FSM programs working with the LSM6DSV sensor, all set to AODR/GODR of 30Hz in line with the examples I copied. Tap detect requires significantly higher ODR.  I might also want to run the SFLP at a rate higher than 15 or 30 Hz, so does this mean that I can't run the FSM when running the AODR/GODR at higher rates than 30 Hz or that I simply need to change the FSM program configuration (gulp!) to account for the desired higher rates?

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @KWine ,

Each feature runs at the ODR selected for that feature (the important thing is to set XL / Gyro ODR properly), furthermore each FSM allows a decimation factor to be applied to run the specific program at FSM_ODR / decimator.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster

3 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
October 6, 2023

Hi @KWine ,

Each feature runs at the ODR selected for that feature (the important thing is to set XL / Gyro ODR properly), furthermore each FSM allows a decimation factor to be applied to run the specific program at FSM_ODR / decimator.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
KWine
KWineAuthor
Senior
October 20, 2023

Would you mind specifying which register has the FSM_ODR decimator please?

KWine
KWineAuthor
Senior
October 22, 2023

Nevermind, I see it. Section 7.6 in AN5907.