MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2HH12 working like 1.6kHz@ODR=800Hz

I am evaluating LIS2HH12. Before starting to collect data, I simply reboot it, set FIFO to stream mode (010), enable FIFO, and enable the sensor by setting ODR=800Hz (110). Then I collect 800 samples (each sample=6 bytes, 2 for each axis) by reading ...

mete by Senior II
  • 2132 Views
  • 2 replies
  • 0 kudos

Resolved! STHS34PF80 sensor with Nucleo_l073

I connected the MKI231KA board to the Nucleo-L073 board to test the STHS34PF80.And I downloaded the PresenceDetection_STHS34PF80 example in the MEMS1 package.Afterwards, I ran Unicleo-GUI and connected it to the COM port, but the data was not read No...

PatrickS by Associate
  • 3225 Views
  • 3 replies
  • 0 kudos

[LIS2DUXS12] Set FIFO_MODE when using FSM

I had an idea to start recording accelerometer data in the FIFO by switching to FIFO mode at one point in the Finite State Machine. This would be done by setting FIFO_MODE bits in the FIFO_CTRL register by using the SETR command. However, in the an59...

BD651 by Associate II
  • 1604 Views
  • 1 replies
  • 0 kudos

Pdm mems microphone

Hi team, I am using MP23DB01HP mems pdm microphone.I am new to this PDM DATA format.i know about pcm.Llease provide information and pseudo code for pdm  to pcm  and vice-versa.Waiting for ur response...!Thank u,Alex

LIS3DH output register value less than the set threshold

I use the lis3dh sensor to communicate through SPI, and the sensor settings are as follows:lis3dh_gvWriteReg(LIS3DH_CTRL_REG0,0x90);lis3dh_gvWriteReg(LIS3DH_CTRL_REG1,0x37);lis3dh_gvWriteReg(LIS3DH_CTRL_REG2,0x00);lis3dh_gvWriteReg(LIS3DH_CTRL_REG3,0...

Andy Zh by Associate II
  • 1264 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DH12 Self Test

We are running the LIS2DH12 self test.  After completing the self test we go back and read stat reg 27 it is always returning FF.  We have tried reading it multiple times, but it always returns FF even if no new data is available.

TVale.1 by Associate II
  • 1989 Views
  • 2 replies
  • 0 kudos

Resolved! LIS3DHH ODR variation

 Digital output data rate (ODR) of LIS3DHH is given (typically) as 1.1kHz in the datasheet. Does it mean ODR is not fixed in one sensor or it is fixed in one particular sensor but there is an inter device variation ? In either case, I am confused how...

mete by Senior II
  • 1915 Views
  • 2 replies
  • 0 kudos

LIS3DH conflicting specification in datasheet

Hi,the LIS3DH datasheet (DocID17530 Rev 2) states on page 1 under Features:"Embedded 32 levels of 16-bit data output FIFO".However, on page 19, section 3.6 FIFO:"The LIS3DH contains a 10-bit, 32-level FIFO"Which statement is correct?

ingfu by Associate
  • 2292 Views
  • 3 replies
  • 0 kudos

Resolved! STEVAL-MKI109V3 does not interpret Z axe value

Hello, I'm using the STEVAL-MKI109V3 board in combination with STEVAL-MKI175V1 and trying to read the X, Y and Z values through the serial port using the commands described in the STEVAL-MKI109V3 documentation and I'm unable to see the Z axe value af...

sch0bert_0-1695896750280.png sch0bert_1-1695897086903.png
sch0bert by Associate III
  • 1841 Views
  • 3 replies
  • 0 kudos