STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1563 Views
  • 0 replies
  • 2 kudos

STM32Cube examples

Posted on December 08, 2014 at 19:59I thought it would be instructive to look at the examples using the STM32CubeMX application. The ''Load Project'' dialog only looks for .ico files and I find none in all of the examples. Was this application used ...

hbarta2 by Associate III
  • 1656 Views
  • 3 replies
  • 1 kudos

Timer Encoder Interface

Posted on December 12, 2014 at 15:54Hi, I'm trying to read an encoder using the encoder interface provided by the STM32F3Discovery board. I've set up the peripherals using CubeMX and connected the encoder to the input pins (tried with timer 1 and 2)...

adriano by Associate II
  • 1995 Views
  • 3 replies
  • 0 kudos

STM32F429 two SDRAMs problem

Posted on December 07, 2014 at 21:12Hello everyone, I have used STM32F429 device along with two SDRAMs AS4C16M16S mapped to the two available banks. When the FMC controller was initialized using the generated code from STM32CubeMX with BANK1 initial...

ok2nmz by Associate
  • 1806 Views
  • 3 replies
  • 0 kudos

STM32L152-Discovery and STM32CubeMX

Posted on November 06, 2014 at 13:25When selecting the STM32L152 discovery board in CubeMX the microcontroller is set to STM32L152RC while my STM32L152 discovery board has the STM32L152RB microcontroller. If I understand correctly the older discover...

STM34CubeMX does not start

Posted on October 20, 2014 at 11:39I had CubeMX installed and working fine. Then I updated the application and now all I see is dialog flashing by the says ''Check files''. After that nothing happens. When I start it from a DOS box I get: java -jar ...

CubeMX 4.4.0 unexpected behavior

Posted on October 20, 2014 at 10:58Hi all, Yesterday I tried to align my project developed with CubeMX 4.3.1 to the recent 4.4.0 version.I did itmainly to overcome a SysTickInit issue with FreeRTOS configuration. Since the regenerated project compil...

DD by Associate II
  • 2238 Views
  • 3 replies
  • 0 kudos

CubeMX 4.3.1 - FreeRTOS SysTick and HardFault

Posted on September 29, 2014 at 11:38Hello,I am using the STM32F3 Discovery Board to try out CubeMX for IAR and FreeRTOS.I have encountered the following situation, where the system hangs:SysTick_Handler is never reached. The system hangs in the Har...

George.P by Associate III
  • 3832 Views
  • 6 replies
  • 0 kudos