STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1443 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeIDE issue with G473 and USB Device CDC

Hello,I've found an issue in STM32CubeIDE1.17.0.When creating a project with USB Device used as a CDC Class and FreeRTOS an include is missing in app_freertos.c:#include "usb_device.h"The project runs properly, but a warning is issued at compile time...

zeboss49 by Associate III
  • 2670 Views
  • 4 replies
  • 0 kudos

No source available for uwtickprio() at 0x20000004

It worked fine until yesterday, but the program seems to have been updated today, and I've been getting that error ever since.The same problem occurs when all the codes are cleared and only the initial init function is executed.I wondered if it was a...

Jins_0-1728287045660.png Jins_1-1728287143183.png
Jins by Associate
  • 2722 Views
  • 4 replies
  • 1 kudos

Resolved! "Command Shell Console" stopped opening (CubeIDE).

After one of the program updates, the "Command Shell Console" stopped opening.As usual, I click on "Open console" button, then on "Command Shell Console", but nothing happens.I rebooted the computer, restarted the program. But nothing changes - just ...

OKhar1_0-1733790502860.png
OKhar.1 by Associate II
  • 2781 Views
  • 4 replies
  • 1 kudos

Unable to use SWV Data Trace Timeline Graph

Hello,I want to use SWV Data Trace Timeline Graph but when I try to open "Configure trace" option, nothing happens, not a single window is being opened etc. Is it some kind of bug, does it have a solution? Thanks in advance.My IDE and other informati...

ozzdemir by Associate II
  • 7849 Views
  • 8 replies
  • 3 kudos

TrustZone: Debugging non-secure doesn't work

Hi,For context I am using the onboard ST-Link from the H563ZI Nucleo board (this one https://www.st.com/en/evaluation-tools/nucleo-h563zi.html). I am using a STM32CubeIDE demo code with IAR from here: https://www.st.com/en/embedded-software/x-cube-fr...

Grailler_1-1734026630915.png Grailler_2-1734026702694.png
Grailler by Associate
  • 1394 Views
  • 0 replies
  • 0 kudos