Skip to main content
Semer CHERNI
ST Employee
Jul 7, 2025 9:33 AM UTC
Question

STM32CubeIDE 1.19.0 released

We are pleased to announce that the release 1.19.0 of STM32CubeIDE is available.

What is new in 1.19.0:

  • Microcontroller, microprocessor, and board lists aligned with STM32CubeMX v6.15.0:
    • Added the support for STM32MP21xx microprocessors to the STM32MP2 series and extended the support for boards based on the STM32MP2 microprocessors
    • Added the support for STM32WL30xx and STM32WL31xx microcontrollers to the STM32WL3x line
  • Added automatic external memory loader prefilling in debug configuration for boards based on the STM32N6 series
  • Added the support for OpenSTLinux 6.1.0 through the update site mechanism
  • Added the support for STM32MP2x-M33-TD projects generated from STM32CubeMX standalone
  • Added the Cortex®-A35 support in the SFRs view
  • Added the capability to install OpenSTLinux through the update site mechanism on empty projects for STM32MP1 and STM32MP2 devices
  • Added the support for TF‑M projects debugging for STM32MP2x-M33-TD
  • Added the new view Flash memories programming allowing the programming of a TSV file for STM32MP1 and STM32MP2 devices in single or dual storage
  • Added the support for new reset strategies when debugging with SEGGER J-Link
  • Added incremental programming as an experimental feature for a defined set of devices:
    • Internal flash memory programming is tested on the following microcontrollers:
      STM32C03xxx, STM32C05xxx, STM32C09xxx, STM32F101/F102/F103, STM32F37xxx,
      STM32F411xC/E, STM32F72xxx, STM32F73xxx, STM32F76xxx, STM32F77xxx, STM32G03xxx,
      STM32G04xxx, STM32G0B0xx/B1xx/C1xx, STM32G491xx, STM32H50xxx, STM32H523/533,
      STM32H562, STM32H563/573, STM32H723/STM32H733, STM32H725/STM32H735, STM32H730
      Value line, STM32H7R3/7S3, STM32H7R7/7S7, STM32L05xxx/L06xxx/L010xx, STM32L4P5/Q5,
      STM32L4x1, /STM32L475xx/STM32L476xx/STM32L486xx, STM32L5, STM32U0, STM32U3,
      STM32U535/545, STM32U575/585, STM32U595/5A5, STM32U599/5A9, STM32WB35xx/5xxx,
      STM32WBA52, STM32WBA54/55, STM32WBA62, STM32WBA63, STM32WBA64/65, and
      STM32WL
    • External flash memory programming is tested on the following boards:
      STM32H735G-DK, STM32H7S78-DK, STM32H573I-DK and STM32U575I-EV

Main fixed issues in 1.19.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x 

Known problems and limitations in 1.19.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x 

How to get STM32CubeIDE 1.19.0:

  • Under this link
  • Or update your current installation of STM32CubeIDE using: Help > Check for updates (The intool update does not allow updating the drivers and STLINK server tool. Full installation is required for this to be done).

 

 

This topic has been closed for replies.

10 replies

Associate
Jul 8, 2025 6:09 AM UTC

Hello, @Semer CHERNI 

 

but the code is not generated in STM32CubeIDE 1.19.0.

Pavel A.
Jul 8, 2025 9:07 AM UTC

> Added incremental programming as an experimental feature

Could you explain this feature please?

 

CTapp.1
Senior III
Jul 9, 2025 11:11 AM UTC

The limitations include:

171852The implemented toolchain is allocating to an enum type only as many bytes as it needs for the declared range of possible values.

Do you have any more information on this, such as a link to a forum post?

This may well be the result of a valid compiler optimisation and not an issue.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Pavel A.
Jul 10, 2025 5:48 AM UTC

Try to build this program to see what is the size of enum by default:

typedef enum {
 foo = 1,
 moo,
 goo,
} E;

int main() {
 E x = goo;
 return (int)sizeof(E);
}

Some GNU compilers by default allocate enum variables as ints. If you specify explicit option -fshort-enums  or -fno-short-enums the result will differ. The question is what of these should be the default (when none options are specified).

CTapp.1
Senior III
Jul 10, 2025 7:39 AM UTC

Thanks, so the issue is really saying that the default behaviour would be to constrain the implementation-defined behaviour beyond what the C Standard does (i.e. either "always use smaller types when the enum fits" or "never use smaller types")?

The use of  -fshort-enums may not be a good default though, as it can cause problems as it results in code that is not ABI compatible with code that doesn't use it (so watch out when linking with code built outside of the project, and don't use it per-file).

Another reason it will be good to get the GCC version up to one that supports C23, as enum base types will then be supported in a portable way:

enum E : uint8_t { ... }

 

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Associate
Jul 10, 2025 3:15 AM UTC

Description Resource Path Location Type
Project XXX has no explicit encoding set

Ctrl+1 working, but the project is not generated

Pavel A.
Jul 10, 2025 10:49 AM UTC

Here you can get a toolchain that has GCC 14.3 with C23 (-std:c23).

It can compile enum: uint8_t  ... but  does not impement _BitInt ?!

 

 

Associate
Jul 17, 2025 10:13 AM UTC

hello, 

regarding Segger new reset strategies, do you have any other document or info to dive more how this new strategies are implemented.

In our case we are using a custom board with a stm32mp153c and reset strategy in production mode is more complex because of binary load using remoteproc from linux side.

Are this new segger strategies adapted to stm32mp1xx ?

 

thanks.

Associate III
Sep 18, 2025 7:14 AM UTC

Hello,

This new revision does not work for me:

C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procédure spécifiée est introuvable
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32.dll
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt.dll
C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procédure spécifiée est introuvable

Do you have any suggestion?

Best regards

Mich

PHolt.1
Senior
Oct 4, 2025 11:44 AM UTC

Does this version fix

- random file opening when doing a Build

- bugs in SWD debugger operations (barely usable SWV ITM and Stat Profiling)

- 10kbytes/sec memory leaks during SWV ITM debugs

- defective error handling of USB debugger (memory usage grows to ~1.5GB and then Cube crashes)

- partly functional STLINK V4 MINIE support (barely working SWV ITM etc)