STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1658 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 621 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STLinkUpgrade - 'Upgrade' button greyed-out

Hello, while trying to flash some test code, I have to run update on STLink, but the "Upgrade" button is not clickable...? I have my board connected, I can see is using lsusb command on my Ubuntu... "Open in update mode" also doesnt give any proper o...

05.06.2026_14.49.20_REC.png 05.06.2026_14.56.13_REC.png
dennis_m by Associate II
  • 92 Views
  • 6 replies
  • 2 kudos

[Solved] STM32Cube IDE Icon Missing on Fedora 41

Subject: [Solved] STM32Cube IDE Icon Missing on Fedora 41Message:Hi everyone,I recently upgraded to Fedora 41 and noticed that the STM32Cube IDE icon was missing. After some searching, I found a solution on Reddit that worked perfectly. Sharing it he...

CubeIDE & MX in MacOS "assessment mode" - for exam use ?

Split from Open-source educational IDE for STM32 – feedback from STM32 users (by @Moussa1492)  for better visibility of this different questionMacOS has an "assessment mode" which blocks any other apps from running.  What I need is the CubeIDE and MX...

phm by Associate II
  • 211 Views
  • 9 replies
  • 0 kudos

Multiline selection not visible after MacOS 26.2 update

It seems that after I updated MacOS to Tahoe 26.2 the IDE does not show selected text if over multiples lines correctly. This is a nightmare to work with, as it does not show selected text and can make you delete (overwrite) lines while editing.Anyon...

snigg by Associate III
  • 983 Views
  • 12 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.