STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1441 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Different hard faults on STM32H562

I have a problem here:When calling strcat() on a target string with odd length and odd source, the controller goes into hardfault, SCB_UFST_UNALIGNED is set. If I deactivate the unaligned trap (SCB_CCR_UNALIGN_TRP == 0), the following happens.The con...

lors by Associate II
  • 1702 Views
  • 3 replies
  • 0 kudos

Problem with using DMA with SPI

Hello everyone,I am currently working on an STM32F411VET6 DISCOVERY board project where I am using DMA for SPI communication with an SSD1331 OLED display. However, I am encountering an issue where the system enters an infinite loop of DMA interrupts....

tospros by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos

Resolved! CubeIDE / MX Download Issue

Hello, i just installed CubeIDE / MX on a brand new Computer. I am running Windows 11.Both IDE and MX have a problem with downloading "software packages" The are extremly slow and after an hour i get an error message. I am not able to work with that ...

Resolved! View Src and Inc files in Project explorer

I have read through a couple posts on this but did not get a clear answer.I have two projects in a workspace.  One shows the tree as:  (This is how I want to see it!)The other just shows Core with only .c files.I can't see what is the difference as f...

FJB2069_0-1733868134096.png FJB2069_1-1733868290939.png
FJB2069 by Senior
  • 2044 Views
  • 2 replies
  • 1 kudos