I had a blue pill board STM32F103C8T6 programmed with the Arduino DFU bootloader and I was able to progam the device using dfu-util (under MacOS) using the Arduino IDE.I would like to switch to STM32CubeIDE to develop an application for the board. No...
I am making a DFU for stm32f4-discovery board.My DFU is using a project generated by STM32CubeMX V1.0. And It worked well with the program generated by the STM32CubeMX V1.0But when I worked with a project generated by STM32CubeIDE, I cannot make the ...
I have a NUCLEO-L4R5ZI board with an STM32L4R5ZIT6P MCU. I have been successfully building and debugging using CubeIDE 1.9.0 with a USB connection to the onboard ST -LINK debugger. However, I've suddenly encountered a situation where after the debug ...
Hello. I work in CubeIDE 1.9.0 with the stm32f429i-disco device. The problem arises about firmware and debugging. I made a simple example to check. During debugging, strange behavior was noticed when executing HAL_Delay (line 95). When executing Step...
Hi everyone!I have to implement a dual bootloader system on different stm32 microcontrollers in STM32cube ide, and I have some questions…The idea is the following:There is a “pre-bootloader�? at the beginning of the flash. When it starts, it gets som...
Hi, I have a challenge about IDE configuration and build steps to make a clean new project.The context is the following : I have a device including 2 micro-controller, 1x STM32F303 and 1x STM32F101. The F303 communicates with the serial bootloader in...
Hello,I am building a project using a batch script which is calling stm32cubeidec.exe to build the separate entities. The project contains a bootloader as well as main application code. I am wondering the best way to combine the two binary files in t...
I am using an STM32 system with separate bootloader and application parts implemented. This time I want to modify and debug the application part, but I don't know how to achieve that in STM32CubeIDE.I would appreciate your advice.*The path of gdb an...
Yet another question on locating data, this time fixed in flash. I want to place some main application attributes at a fixed flash location so that my bootloader can learn about the installed app. I have had partial success. (For now this is for an S...