I flashed the STM32 L152 discovery board with Cube IDE. I assume that if I run/debug the project with board plugged in, it will automatically upload the firmware. However, it shows as File download completeTime elapsed during download operation: 00:0...
If I try to use the import comand, from File menu of STM32CubeIDE, to load an example selecting "import STM32Cube example" option I can't load a project only available in source form. The window that open, were we have a list of available projects fo...
I am using STM32L451RCTx in STM32CubeIDE. I need to response through usart2 for the received request on the same usart2. I am receiving the request one time and can able respond for that. After the transmission of the response, I am not able to recei...
In trying to troubleshoot ADC DMA issues I have built the example code from:STM32Cube\Repository\STM32Cube_FW_L1_V1.10.3\Projects\NUCLEO-L152RE\Examples_LL\ADC\ADC_MultiChannelSingleConversionHowever, when it converts the results it hardfaults due to...
Ubuntu STM32CubeIDE 1.8/1.7File -> New -> STM32 ProjectChoose STM32L100RB -> Next -> Project Name : "removeMe2" -> FinishIn Device Configuration Tool: Pinout&Configuration -> Connectivity -> SPI1 -> Mode: Full Duplex Master Project Manager -> Advan...
Hi , i am new to some of the peripherals of STM32 controllers...I am using STM32L151RCT6 MCU in STMCube IDE for my application..My requirement is like i need to receive the new firmware binary file via Y modem and need to write into the flash and nee...
HI ,I am new to the STM controllers and STM32Cube IDE.While loading the code i can see the only some sectors (i.e from 0 to 30 sectors or 0 to 64 sectors) are erasing and loading the new program...Please suggest me how to erase the complete interna...
Hi ,I not used RTC earlier and new to RTC.I am using STM32L151RCT6 MCU and creating the project in STM32Cube IDE.what are the settings i need to do to get RTC timing of 12 sec..I searched and got some information about alarm time setting and alarm in...