STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-L475E-IOT01A2 - When using the XCUBE-BLE2 pack it seems that MCU hangs when the code resets the BLE module during initialization

Hello,I use the B-L475E-IOT01A2 board and I try to integrate/experiment with the BLE module.I created a new project using the STM32CubeIDE where I let the IDE apply the basic configuration for the board.Then I select the BLE2 pack which I configure t...

BLE project missing files STM32CubeIDE V: 1.7.0

Hello,I'm trying to go through some BLE examples and found some out dated videos on the web. I understand there have been changes over the last year or so but one thing I cannot understand, is missing files.When creating a BLE project in CubeIDE, it...

kcire L. by Associate III
  • 240 Views
  • 3 replies
  • 0 kudos

BLE_Beacon Example on STM32CubeIDE and P-Nucleo WB55

I'm trying to make the "BLE_Beacon" example found inside the "STM32CubeWB" file work with the STM32CubeIDE and the P-NUCLEO WB55 board. The program compiles correctly but I can't see the beacons. Debugging I saw that when it arrives in the loop it cr...

MVegl.1 by Associate
  • 407 Views
  • 4 replies
  • 0 kudos