STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 with External QSPI Flash & SDRAM execution

I am using STM32H7xx MCU with External QSPI Flash and SDRAM.I want to download my code using STMCubeIDE directly to External QSPI Flash and once done I want to execute the same code from SDRAM without compromising the debugging ability using STMCubeI...

DPila.1 by Associate II
  • 1190 Views
  • 5 replies
  • 0 kudos

STM32H735 QSPI init failed with NCS pin disabled

preconditions:CubeIDE 1.11.0 configured QSPI with disabled NCSenabled: Project Manager-->Code Generator-->HAL Settings-->Enable Full AssertThe idea is to have multiple QSPI chips connected to the QSPI with their own chip select pin. So the use NCS sh...

0693W00000WLBinQAH.png
MStei.4 by Associate III
  • 212 Views
  • 0 replies
  • 0 kudos