STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fault input for HRTIM is configured as output?

Hi, I am working with the HRTIM in the STM32G474 Nucleo and trying to configure the fault input to reset the outputs.When I see in the GPIO config of the HRTIM in the STM32CubeIDE I see that the fault input pin HRTIM_FLT1 is configured as Alternate F...

DKuro.1 by Associate III
  • 210 Views
  • 2 replies
  • 0 kudos

Fault input for HRTIM is configured as output??

Hi, I am working with the HRTIM in the STM32G474 Nucleo and trying to configure the fault input to reset the outputs.When I see in the GPIO config of the HRTIM in the STM32CubeIDE I see that the fault input pin HRTIM_FLT1 is configured as Alternate ...

DKuro.1 by Associate III
  • 213 Views
  • 0 replies
  • 0 kudos