STM32CubeIDE (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to solve strange hard fault issue

Building a custom board, which can accept either an STM32F205 or an STM32F405. Have boards with both MCU built. System running FreeRTOS 10, with three tasks total.Embedded software has shared application code between the two builds, only the stuff ge...

MClar.3 by Associate II
  • 712 Views
  • 7 replies
  • 0 kudos

Resolved! how do i change the driver?

I'm using NUCLEO-207FZGIn cubeIDE, HAL driver is provided by default.I want to change to the SPL(Standard Peripheral Library).Since I am a beginner, I would like to get tips. Before you try, ask a question.I wonder if it is enough to simply add the S...

Psang.2 by Associate II
  • 319 Views
  • 2 replies
  • 0 kudos

I will try to ping another ip with STM32F207VG.

I pinged STM32 with my PC.However, STM32 did not find a way to ping another ip.Ask for advice.I am using STM32F207.I'm using STM32CubeIDE.I am using FreeRTOS.I called functions in api_lib.c to connect the network.The PC pinged STM32 and the response ...

Lyoun.1 by Associate
  • 140 Views
  • 0 replies
  • 0 kudos

How to change VECT_TAB_OFFSET in IDE (MX)

Now, I develop DFU.0x80000000 : DFU Project0x8000C000 : Application Project.I have to change VECTOR Table in Application Area.I'm trying to find VECT_TAB_OFFSET in IDE.But, I can'tOld solution is directly change source code in System_stmf2xx.cI don't...

NH by Associate II
  • 848 Views
  • 6 replies
  • 0 kudos

I am developing a series of NUCLEO 144-based project around my house, the principle point being that they're Ethernet-connected. I'm using the NUCLEO F207ZG as a first device, and the STM32CubeIDE. Is that the right place to start?

I'm after some advice. I've just discovered the STM32 NUCLEO boards, and I've used many MPUs (Atmel, Microchip, TI) in the past. I'm a fairly experienced software developer, but this is strictly homer stuff.I've been trying to get the FreeRTOS/LWIP d...

AWard.1 by Associate
  • 206 Views
  • 2 replies
  • 0 kudos