Resolved! STM32CubeIDE Licence for all STM32 MCUs
Hi Team,Can you please help me regarding the licensing of STM32 MCU for CUBE IDE? is it required or free for all STM32 MCU?Regards,N.Anwar
Hi Team,Can you please help me regarding the licensing of STM32 MCU for CUBE IDE? is it required or free for all STM32 MCU?Regards,N.Anwar
HAL_UART_Receive and HAL_UART_Receive_IT contain a bug. To reproduce (I use STM32L412KB nucleo 32 for this):Connect a terminal emulator to the ST-LINK as serial port.Configure that serial port in CubeIDE if default not chosen.Use for example the foll...
Hi!I'm currently using a Nucleo-L432KC board to move a servo. There's a pin connected to the Servo (PA_8), a pin for a button interrupt (PA_4) and a pin for a LED indicator (PA_6). The issue arises when I call the following function:void HAL_GPIO_EXT...
Hello. When I press to Run (Run main.c) button, STM32CubeIDE opens random file, possibly, from current repository, for example: startup_stm32l452xx.s, core_cm4.h etc... Code is loading successful, but this side effect bothers me. I would like to dis...
I tried: import/general/existing projects from workspace, thenchoose nucleo-l452re/examples/gpio/pgio_iotoggle,I get the whole file structure, get my main.c, see the file, however, the "hammer" is greyed out. Cannot be built. What is wrong with these...
Hi Guys,I'm writting a bootlader/application for STM32L4 in STM32CubeIDE i I want my app to run even if there is no bootloader in memory. This is my *.ld file:/* Memories definition */ MEMORY { RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 96K ...
Hi,I was looking on some tutorials to do FFT on the NUCLEO-L476RG board, where they recomended using CMSIS DSP library. The DSP configuration guide from ST (link below) said to add the library path under Project Properties ->Tool Settings ->GCC Linke...
Hello,My name is Ray.I'm an end user that come from Taiwan,I'm still learning coding with stm32Recently i encounter a problem about debug via STMCubeIDE,The version is 1.15.1Once i coding fine and process into debug mode,it will perform a full chip ...
I have win forms GUI and sending data from this GUI to STM32 Nucleo L4R5ZI µC over UART in byte array format. After receiving data over UART in µC, I am converting the data to their native formats such as Int ad Float. I don't have issue converting i...
I have followed the eeprom emulation described in X-CUBE-EEPROM expansionhttps://www.st.com/en/embedded-software/x-cube-eeprom.htmlBut the solution was written using the old STM32 standard API. Does somebody knows about an EEPROM Emulation solution t...