Convert Arduino code to STM32 IDE code
Hi,I would like to convert Arduino code to STM32 IDE code.Could you please suggest for me ?Thank you
Hi,I would like to convert Arduino code to STM32 IDE code.Could you please suggest for me ?Thank you
I have already spent hours trying to get the Arduino library working in my CubeIDE (1.12.0 IDE; latest STM32duino; Firmware F3 1.11.4). I set up all the include paths, and changed the arduino stuff, to point to the CubeIDE generated files. I had some...
I had a blue pill board STM32F103C8T6 programmed with the Arduino DFU bootloader and I was able to progam the device using dfu-util (under MacOS) using the Arduino IDE.I would like to switch to STM32CubeIDE to develop an application for the board. No...
I see Nicla Vision board having lot of potential but the board in and of itself cannot do enough.In order to open its potential, it should be able to talk to existing STM32(STM32F407 for e.g.) based boards through either SPI or UART interface.Do we h...
I made a test code in arduino to read SSI. How can I make the shiftin function work correctly in the stm32 controllers? . In the stm32cubeIDE I can't manage to make it work like in the arduino ide.In the shiftin function the variables: data_pin, cloc...
Hi all!I used to "work" with Arduino environment in the past. Now I passed to Eclipse based IDE and in this specific case I'm using STM32CUBEIDE to develop a C project for an F100 series MCU. In the Arduino world I used often a library written in C++...
I'm trying to use the Led strip w2812b for a project because i want to add it to an existing project, the support for the arduino is very good and since my code is already in stm32cubeide i cant port to arduino ide. Is there any way to use the FastLE...
Hello everyone! I'm new in stm32 and I should program an stm32f100 using the STM32Cube IDE. My board should drive an lcd (st7565r controller via 4 wire SPI) and 4 push button, and communicate on a Modbus line as master. Actually my code on Arduino r...