STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! No basic BLE HID examples!

Hello, for many years there are only 2 basic HID devices - keyboard and mouse and more recently - keyboard mouse combo! Is there any reason for not providing there examples? I guess that half of employees can do that task if this is so easy and obvio...

GS2 by Senior II
  • 3567 Views
  • 6 replies
  • 1 kudos

Resolved! Elf file and relative paths

I'm working on the STM32WL55 Nucleo-64, starting from the LoRaWAN_End_Node.I performed a hexdump and noticed that the ELF file generated at the end of the compilation process contains a significant recurrence of absolute paths, as shown in the pictur...

Feanoer_0-1720519174226.png Feanoer_1-1720520553204.png
Feanoer by Associate II
  • 4081 Views
  • 6 replies
  • 2 kudos

Resolved! How to running a FUS when using UART

Hi, I am using a STM32WB15 board for BLE applications. I understand I need to download the correct FUS before I can ask the board for running any programme. However, I find when using UART to connect the board I cannot running the FUS as well as wire...

Resolved! Unble to read the Wireless satck Name in STM32WB

Hello,I want to read which stack is updated in my controller. For example stm32wb5x_BLE_Stack_full_extended_fw / stm32wb5x_BLE_Stack_light_fw / stm32wb5x_BLE_Zigbee_RFD_static_fw. So can I read back the stack name using code? Is there any way to read...

Smalik by Associate II
  • 1515 Views
  • 1 replies
  • 0 kudos