Have anybody developed BLE HID sample?
Have anybody developed BLE HID sample for P-NUCLEO-WB55 board ? I am very interested in Keyboard or Mouse or better Combo code.
Have anybody developed BLE HID sample for P-NUCLEO-WB55 board ? I am very interested in Keyboard or Mouse or better Combo code.
I have seen videos or examples of stm32wb workshops, but I have seen most of them send and receive data such as sensor data or LED control through the Android app of st.In the past, when I used an external BLE module(BM70 of MICROCHIP) , I could send...
Hi everyone.im trying to create a project with a LoraWan module that based on stm32wle5ccu6.(RAK3172).after compliting my ioc UI i build the project, on the building process i got this error./LoRaWAN/App/lora_app.c:33:10: fatal error: adc_if.h: No su...
Hello,I have started to use stm32wl55 nucleo.I try to debug a basic application.I start by debugging CPU1 (CM4) than after booting CPU2 (CM0+) i run the debug for the second CPU.But ST-LINK: Could not verify ST device!error details :Error in final la...
Hello, I have a problem running any project in STM32CubeIDE v1.7.0When I press 'Run' I usually get "Launching: Performing pre-launch check..." and it just hangs there.Sometimes it gets past that, and then I get the following errorError in final launc...
Hi all. Let me tell you the problem I'm facing and I googled for finding some help but without luck. The problem I have in hands is as next. I was using Nucleo WB55 to use the STM32F103CBT6 to program a microcontroller I have in a custom PCB for an e...
Hello Thank you for your help always I hope for a positive reply on this because it has indeed stressed me for some good time please help me Am using a temperature sensor and I want to be receiving the sensor values from the st ble toolbox app every ...
I have connected a Nicerf SX1262 us915 lora module with the STM32L496RG MCU. Lora module has DIO1 and Busy pins for tx and rx confirmation(data send and receive ).I'm using STM32CubeExpansion_LRWAN_V1.3.1 library and i have used sx1262 example which ...
Hello,I run STM32WB exemple : BLE_p2pServer_ota on STM32CubeIDE with the BLE_Ota exemple for bootloader. In this application we start from address 0x08007000MEMORY{FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 484kRAM1 (xrw) : ORIGIN = ...
Hi all,I hope you're doing well. I'm working on a project with the STM32WB10CCU5 microcontroller and could use some help with setting up an OTA (Over-The-Air) update handler. I've searched through docs and examples but can't find a fit. Most resource...