STM32 MCUs Wireless

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to flash Wireless Coprocessor Binaries with STM32CubeProgrammer? Trying to flash the STM32WB5MMG Bluetooth module on a B-U585I-IOT02A (STM32U585AI) board.

Hello!I'm currently trying to get two B-U585I-IOT02A (STM32U585AI) boards to communicate with UART over BLE. I'm using the BLE_CableReplacement example project (STM32Cube_FW_WB_V1.13.3/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE/BLE_CableReplaceme...

juyec by Associate II
  • 709 Views
  • 8 replies
  • 0 kudos

Resolved! Wifi on B-U585I-IOT2A using SPI

Hello, I'm working on the Wifi on the board B-U585I-IOT2A. I'd like to connect 2 modules, including the microcontroller, to the same wifi so that they can communicate with each other.I've made some research about Wifi MXCHIP EMW3080 and example HTTP_...

AI_STM by Associate II
  • 203 Views
  • 3 replies
  • 2 kudos

Resolved! STM32WL5M

I attendded a trainning last year on STM32WL5M, we were told this product will be available 2024 January. I have been checking but looks like is not available.Do anyone have information when this product will be available?

STeng by Associate
  • 326 Views
  • 5 replies
  • 1 kudos

Trying to interface with STM32WB on B-U585I-IOT02A

Hello,I am trying to comunicate the STM32U5 of the board with the STM32WB module, as I need a star network (1 client with 5 servers), I could also use a mesh. To comunicate different nodes. I am having trouble with it, as I just send basic "AT+BLE_RS...

VCasa3_0-1702673869786.png
VCasa.3 by Associate II
  • 169 Views
  • 0 replies
  • 0 kudos

How to set up BLE AT Client on B-U585I-IOT02A?

Hello!I'm attempting to set up the BLE AT Client example in the STM32U5 firmware package on a B-U585I-IOT02A board. I've managed to flash it, but when I run it on the debugger (through the ST-Link v3 USB port), the "AT" and "AT+BLE_SVC=1" commands se...

juyec by Associate II
  • 319 Views
  • 2 replies
  • 0 kudos

How to send AT commands through UART on B-U585I-IOT02A?

Hello!I have a question - I'm working on interfacing with the STM32WB5M module on the B-U585I-IOT02A. From what I understand, the STM32WB5M module is already flashed with an example for AT commands (in the STM32Cube_FW_WB_V1.13.3/Projects/P-NUCLEO-WB...

juyec by Associate II
  • 736 Views
  • 4 replies
  • 0 kudos

How to configure BLE from STM32U5 MCU pinout (IOC file)?

Hello! The title pretty much says it all - I'm trying to figure out how to configure BLE between two B-U585I-IOT02A boards, but establishing the BLE connection is a bit confusing to me. Am I able to configure it from the UFBGA169 IOC file in STM32Cub...

juyec by Associate II
  • 666 Views
  • 6 replies
  • 0 kudos