STM32 MCUs Wireless

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Slow block read with SPI fatfs

Hello,I measured the performance of uSD card connected through the SPI on Read/Write operation.The weird thing is that the Block read speed is 3x to 4x slower than the write speed.  I'm writing/read 4kB of data and the SD card is formatted with 4kB a...

frnt by Senior
  • 572 Views
  • 12 replies
  • 0 kudos

Having issues enabling the SubGhzSPI on STM32WLE5JC

I have five identical development boards that I am attempting to bring up. One of the boards works without issues. The other four all fail during MX_LoRaWAN_Init(), After digging a little deeper I found that the SubGhzSPI peripheral is never getting ...

Kurt28 by Associate
  • 561 Views
  • 7 replies
  • 3 kudos

SPI MISO line stays high?

I am writing a driver for the STM32 to get the data from the front-end board, AD5940 using the SPI communication. I am using the AD5940 library available at the : https://github.com/analogdevicesinc/ad5940lib.STM32WB55xx has been used. I have configu...

HJain.3 by Associate
  • 578 Views
  • 2 replies
  • 0 kudos