Resolved! STM32-WB55RG without USB dongle
Does STM32-WB55 MCU work without USB dongle? Where can i find the quick start program for led blinking ?
Does STM32-WB55 MCU work without USB dongle? Where can i find the quick start program for led blinking ?
I AM USING STM32 WL55JC2 CONTROLLER TO WORK AS A LORA END NODE , I AM WORKING WITH EXCISTING CODE FOR LORA END NODE AND I WANT TO CONFIGURE UART1 , THE CODE IS WORKING UNDER SEQUENCER OS. SO I AM TRYING TO IMPLEMENT UART1 WITHIN THE SEQUENCER OS , U...
Hi, I have two NUCLEO-WL55JC1 boards with me. I want to make one board as a end device and one board as a gateway. I found end node example with in firmware package of STM32WL but not found any example for gateway.Is there any gateway example availab...
The STM32WL55 JC modules are taking 4 seconds time to switch from Receiver mode to transmitting mode, can you please give some information that how can i reduce that switching time. https://github.com/stm32-hotspot/STM32WL-SubGHz-Phy-Rx-Hop Used th...
Before writing, I apologize for the unsophisticated use of English. Hello, I'm student who struggle with ble. I want to transmit the IMU GYRO Info & Camera Video ( or Image ) by STM32WB Module on the board. But I don't have any idea for starting b...
Dear All,I am search for an example BLE beacon code for the NUCLEO-WB55RG board which solely uses the HCI layer.There is an example for the WBA board: https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA55CG/Applications/B...
Hi,I am currently attempting to debug the secondary core (cortex-M0+) on the STM32WB15CC board, but I have encountered challenges in doing so. According to the documentation, the boot process is initiated by setting C2BOOT through the primary core (c...
STM32WB55RGV MCU is in use, and BLE_HeartRateFreeRTOS example is under review. In the example of BLE_HeartRateFreeRTOS, it was confirmed that the STOP2 mode function was included, but I don't know the Stop mode entry conditions.And I wonder if I can ...
Dear St,I'm developing a cluster with a client and server, where I have a client to write on the cluster of the server. I can write with the function ZbZclWriteReq() on the server, but I'm not always successful. When I do the first write, I have succ...
Hi team, Warm GreetingsI am using STM32WB55RG6VTR controller in our battery operated product development. We are enabling the sleep mode in the controller to test the current which is around 10mA but it is supposed to be around 40uA if all peripheral...