Resolved! Zephyr support for STM32WB09
Are there any plans to add Zephyr support for the STM32WB0X line of chips? Or is it already supported with the current HAL? I couldn't find any Zephyr related information on the product page.
Are there any plans to add Zephyr support for the STM32WB0X line of chips? Or is it already supported with the current HAL? I couldn't find any Zephyr related information on the product page.
Hello,I want to use STM32WB55 with Zephyr to communicate via openthread network. Which FW Version of co-processor is working. I want to use stm32wb_Thread_FTD_fw.bin as co-processor FW. On: github.com/zephyrproject-rtos/zephyr/issues/47991 is said th...
Hello,I am playing with NUCLEO-WB15CC board + zephyr + BLE beacon example. After compiling and flashing the example to the board I got "Precise data bus error" during Bluetooth initialization.Because zephyr does not support stm32wb15 out of the box, ...
Hi allSTM32WB55RG nucleo board zephyr (3.0)When BLE stack is enabled, it becomes halt.Can't I use LSI clock to make the BLE stack run ?We made a sample board, but We didn't attach an LSE.So. use LSI clock. If We use LSE in nucleo , it will behave...
Hello!I need to consider the best BLE stack firmware for production and its release provided by STMicroelectronics.Is there some long term version or some release that have long term support status?Are there some plans in BLE stack firmware developme...
I am tying to develop an application in Zephyr for a battery powered device that goes into STOP2 mode for low power consumption when advertising. I have successfully created a test app with STMCube based on the health thermometer example which does t...