STM32 MCUs Wireless

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SAI: Won't stay enabled (H7 and WB)

Hi - I'm having a real struggle with the SAI peripheral. I've tried on both H742, and WB55 module, and am running into the same problem.I have the source set up in the clock config (Tried both PLL1 and PLL2, and using PLLSA1P on WB), and made sure I ...

DOCon.1 by Senior
  • 275 Views
  • 4 replies
  • 0 kudos

Using stm32wb core M0+ for user program

Hi,I am looking for a dual core controller and options I have been able to find out are:Stm32Wb seriesStm32H seriesBeing, H series quite expensive, Is it possible to use WB series M0+ for running another application in parallel?Or we can only use it ...

AKuma.33 by Associate II
  • 152 Views
  • 1 replies
  • 0 kudos