STM32 MCUs Wireless

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I have STM32WB55. It has 1 UART and 1 low-power Uart (lpuart). I can see Zigbee uses lpuart, as there is no UART left, is it possible to use on STM32WB55 Nucleo board Zigbee and sensor whit SDI12 protocol?

Hi, I have STM32WB55.It has 1 UART and 1 low-power Uart (lpuart). And I have SDI12 sensor.I have successfully read whit lpuart SDI12 protocol sensor. But now I want to use ZigBee to send data that I read from the sensor to the Zigbee coordinator. I c...

Nja.1 by Associate II
  • 508 Views
  • 1 replies
  • 0 kudos

How to make traces work with Steval-Proteus1 (LPUART1)

I'm new to working with STM32, and I'm having issues getting some kind of output to the console (have been using both Tera Term & the built-in console in STM32CubeIDE) when working with the Steval-Proteus1 board. I tried following two seperate guides...

_legacyfs_online_stmicro_images_0693W00000dJpy2QAC.png _legacyfs_online_stmicro_images_0693W00000dJpyQQAS.png
NGrun.1 by Associate
  • 253 Views
  • 0 replies
  • 0 kudos

RAK3172 LPUART sample code-LED not litting?

I am checking the below example code given in RAK3172 low level development folder.C:\en.stm32cubewl\STM32Cube_FW_WL_V1.0.0\Projects\NUCLEO-WL55JC\Examples_LL\LPUART\LPUART_WakeUpFromStop_InitThe only change I made here is for LED2 , GPIO pin changed...

PP.3 by Associate
  • 229 Views
  • 1 replies
  • 0 kudos

STM32WLE5 wake up from stopmode using LPUART with LSE

Hello, to get a lower power consumption in my application i would like to go in stop mode 2 and wake up shortly to receive some characters on the LPUART. But unfortunately my mcu does not wake up. I can see with the debugger that the send Byte is in ...

APell.3 by Associate
  • 197 Views
  • 0 replies
  • 0 kudos

STM32WB5MMG, is there a ZigBee Touchlink Example?

Hi all,I try to implement a ZigBee device that acts as a Touchlink Target.My hardware is a STM32WB5MMG module. My debug UART is the LPUART1, no other UART configured.I use the STM32CubeMX 6.6.1 to generate the project and STM32CubeIDE 1.10.1 to compi...

TThan by Associate III
  • 303 Views
  • 2 replies
  • 0 kudos

Resolved! Disable VCOM in SubGHz_Phy middleware

Hello,I would like to disable the LPUART in my project to save power consumption. I am programming a point to point network with LoRa modem. My project is based on the ping pong subghz example.Curently, my board consumes around 107 µA in sleep with t...

nogema by Associate II
  • 369 Views
  • 3 replies
  • 0 kudos