cancel
Showing results for 
Search instead for 
Did you mean: 

RF matching network _ Z values _ nucleo RF performance

malarab
Senior II

Hi,

I started a Circuit/PCB design with STM32WL55CCU (UFQPN48) to work at 433MHz.

I was referred to ST design for low band/Hight power and to AN5457.

But I am style missing for some information:

  • What is the PA impedance at 433MHz for UFQPN48 package?
  • In AN5457, the recommended value of L6 between 300MHz and 500MHz is 68nH. Why in all ST circuit design (low band) L6 is set to 56nH?
  • Is the order of C4 and L3 has any influence on the circuit (some time C4 is before L3, and some time C4 is after L3)
  • In the different ST circuit design, the CLC PI filter an matching (C8/L4/C7) is not accorded to 50ohm. Is it normal?

…..

After making some test with the nucleo board wl55, I cannot find the same range like I had with other RF433 module. It is look like RF circuit is not optimised or …. Is anybody have the same observation?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tve
Associate II

I'm having the same questions about PA output impedance at 433Mhz and I also noticed the L6 discrepancy. Would be nice to have some answers...